(3)| 6/20/2021 10:45 AM | |
|
Posts: 8092 Rating:
|
Hello, Please refer attached project of controlling 6RA70 DC drive on Profibus by PLC S7-300. Used simple instrunctions (for better understanding) & only drive related inputs/outputs are configured. Additional DI/DOs are available for interfacing more I/Os. Object of this tip is to help user to understand basic concepts of how to establish communication & transfer/receive basic data. HTH. Attachment6RA70 - PLC.zip (2197 Downloads) |
This contribution was helpful to
|
|
| 8/6/2021 2:32 PM | |
|
Joined: 7/6/2020 Last visit: 4/18/2025 Posts: 23 Rating:
|
Dear Friend, please elaborate MW0, MW16, and MW2, MW6 |
| 8/7/2021 10:13 AM | |
|
Joined: 7/6/2020 Last visit: 4/18/2025 Posts: 23 Rating:
|
Thanks dear for your kind and fast response. but pls have a look the attachment. This create a confusion for me.Attachmentprog.zip (1874 Downloads) |
| 8/7/2021 10:19 AM | |
|
Posts: 8092 Rating:
|
Hello, What confusion do you have? Please explain. Attched file is with .rar extention. Which is project? I cannot open it. |
| 8/7/2021 2:59 PM | |
|
Joined: 7/6/2020 Last visit: 4/18/2025 Posts: 23 Rating:
|
Hi, Pls see the pic 1, in program PQW 256 is taking value from MW0, where as in pic 2, symbol table PQW 256 is addressed with MW2. Why? thanks Attachment1.zip (1809 Downloads) |
| 8/8/2021 10:24 AM | |
|
Joined: 7/6/2020 Last visit: 4/18/2025 Posts: 23 Rating:
|
thanks dear |
| 11/3/2025 9:29 PM | |
|
Joined: 10/17/2007 Last visit: 12/30/2025 Posts: 4568 Rating:
|
If you already made your project working followed the example given by PISCEAN 2010, dont care so much about how to select MW??, I think the expert has his good reasons to do like that way --such as the MW should not being used by the other function in the same PLC project, and also need consider modify (add new function) in the future. I attached control wards from the manual -you can see they occupied 2 words of memory. the words I think used in the example. and some other reasons not important for making project working. Hope this helps you BWT: I did not visit DC drive forum so often, as I see your question stay for a long time, so I give your my suggestion
AttachmentControl_word_function_diag.pdf (23 Downloads) |
|
If you like my comments please |
|
This contribution was helpful to
|
|
Follow us on