(0)| 5/1/2025 5:00 PM | |
|
Joined: 12/18/2014 Last visit: 12/28/2025 Posts: 36381 Rating:
|
PROFINET GSD files: I/O – ET 200SPThis entry comprises the current PROFINET GSD files as a download for the input/output modules of SIMATIC ET 200SP, including PROFIsafe. PROFINET GSD files: Station type:IM155-6PN...,IM155-6MF... (file type: XML)
|
| 7/1/2025 11:37 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Joined: 12/18/2014 Last visit: 12/28/2025 Posts: 36381 Rating:
|
PROFINET GSD files: I/O – ET 200SPThis entry comprises the current PROFINET GSD files as a download for the input/output modules of SIMATIC ET 200SP, including PROFIsafe. PROFINET GSD files: Station type:IM155-6PN...,IM155-6MF... (file type: XML) This GSDML can be installed in the following STEP 7 versions:
This GSDML can be installed in the following TIA Portal versions:
Station types:IM155-6PN...,IM155-6MF... (file type: GSDX, with digital signature) GSDX-V1.0-Siemens-ET200SP-20250606.gsdx.zip (1,5 MB) (SHA-256) The GSDX package provides a container format which allows multiple elements and files (GSDML, bitmaps, etc.) to be packaged into a single resource (package). It can additionally contain a digital signature that ensures integrity and authenticity of the GSDX package. Installation of this GSDX is not possible in STEP 7 Classic. This GSDX can be installed in the following TIA Portal versions:
Change history: 2025.06_History_ET200SP_PROFINET_GSD.pdf (105,6 KB) (SHA-256) Archive versions:
ET200SP_IM155-6_Archivstaende.zip (7,2 MB) (SHA-256) FAQ: How do I define the SHA-256 checksum of a file? 109483101 |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||
This contribution was helpful to
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| 8/24/2025 11:18 AM | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Joined: 12/18/2014 Last visit: 12/28/2025 Posts: 36381 Rating:
|
PROFINET GSD files: I/O – ET 200SPThis entry comprises the current PROFINET GSD files as a download for the input/output modules of SIMATIC ET 200SP, including PROFIsafe. PROFINET GSD files: Station type:IM155-6PN...,IM155-6MF... (file type: XML) This GSDML can be installed in the following STEP 7 versions:
This GSDML can be installed in the following TIA Portal versions:
Station types:IM155-6PN...,IM155-6MF... (file type: GSDX, with digital signature) The GSDX package provides a container format which allows multiple elements and files (GSDML, bitmaps, etc.) to be packaged into a single resource (package). It can additionally contain a digital signature that ensures integrity and authenticity of the GSDX package. Installation of this GSDX is not possible in STEP 7 Classic. This GSDX can be installed in the following TIA Portal versions:
Change history: 2025.08_History_ET200SP_PROFINET_GSD.pdf (105,2 KB)(SHA-256) Archive versions:
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
This contribution was helpful to
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| 10/28/2025 2:38 AM | |
|
Joined: 12/18/2014 Last visit: 12/28/2025 Posts: 36381 Rating:
|
PROFINET GSD files: I/O – ET 200SPThis entry comprises the current PROFINET GSD files as a download for the input/output modules of SIMATIC ET 200SP, including PROFIsafe. PROFINET GSD files: Station type:IM155-6PN...,IM155-6MF... (file type: XML) |
This contribution was helpful to
|
|
| 12/22/2025 6:57 AM | |
|
Joined: 12/18/2014 Last visit: 12/28/2025 Posts: 36381 Rating:
|
PROFINET GSD files: I/O – ET 200SPThis entry comprises the current PROFINET GSD files as a download for the input/output modules of SIMATIC ET 200SP, including PROFIsafe. PROFINET GSD files: Station type:IM155-6PN...,IM155-6MF... (file type: XML) |
This contribution was helpful to
|
|
Follow us on