(0)| 12/24/2025 1:50 PM | |
|
Joined: 4/24/2006 Last visit: 12/24/2025 Posts: 9097 Rating:
|
Hello, You will need a CP343-1 in your S7-300 project. But it is a spare part. Another possibility might be a Gateway. Perhaps: Anybus Communicator – PROFINET IO Device to PROFIBUS DP Device Best regards, Wizard |
This contribution was helpful to
|
|
| 12/25/2025 3:58 AM | |
|
Joined: 12/24/2025 Last visit: 12/26/2025 Posts: 2 Rating:
|
Thank you for reply. please suggest siemens hardware active state |
This contribution was helpful to
|
|
| 12/25/2025 2:20 PM | |
|
Joined: 9/27/2006 Last visit: 12/28/2025 Posts: 12477 Rating:
|
Hello; I am sorry, your last request is not clear. What exacltly are you asking? If you look at the following document (PN/PN coupler, Getting Started) you will see that the coupler allows transmission of data between 2 PN IO controllers, so in your case both the s7-300 and the S7-1500 must act as an IO Controller on their Profinet network. https://support.industry.siemens.com/cs/ca/en/view/88737127 Wizard already posted the standard solution, adding a CP 343-1 as part of the hardware of the S7-300, allowing it to act as an IO controller. For the S7-1500, this functionnality is built-in. Since the S7-300 is an older controller, some of the harware is now only made available as a spare part, which makes it more expensive and difficult to locate. If you have trouble finding it, Wizard proposed another solution, a gateway that will allow the S7-300 to act as a Profinet IO Controller, which would allow you to connect to a PN/PN coupler. Wizard's reply covered your inquiry very clearly, don't you think? Therefore, please clarify your last question. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/25/2025 14:23:46 |
|
This contribution was helpful to
|
|
Follow us on