9/17/2009 4:36 AM | |
Posts: 54 Rating: (0) |
Can i used siwarex ms for a load cells of 10,000 kgs each... 4 loadcell in one tank..................... Pls. see attachment...for load cell characteristic ill be using s7 200 and hmi for this project......just for monitoring....do you think ill have aproblem with its resolution AttachmentAccupoint.pdf (261 Downloads) |
9/17/2009 10:41 AM | |
Joined: 5/28/2008 Last visit: 11/6/2024 Posts: 4516 Rating: (839) |
Hello ivan_euler , I do not think that there would be a problem with Siwarex MS. But I think using standalone integrators would be better for your application specially you need only to monitor the weight. Siemens offers stand alone integrators like BW100 & BW500. Regards, |
Ayman Elotaify |
|
9/23/2009 9:11 AM | |
Joined: 5/28/2008 Last visit: 11/6/2024 Posts: 4516 Rating: (839) |
Dear ivan_euler, Please read carefully the following statement taken from Siwarex MS manual: Weighing Range The maximum weight is defined during adjustment. The “integer” number format limits the entry to a maximum of 32767. The maximum weight depends on the number and type of load cells used. |
Ayman Elotaify |
|
Follow us on