Industry Online Support
Technical Forum
2/3/2010 11:23 AM | |
Posts: 4 Rating: (0) |
Hi, I'm trying to configure a 2oo3 voting system using SIL 2 compatiable transmitter to give me a SIL 3 rating for the loop can anyone help on how to configure this in the SET. I've attached my project so far and the loop in question is the one named 'Water Drum Level'. Also under the REACTION heading I'm trying to input several solenoid operated shutoff valves in series to increase the SIL level and am unsure how to accomplish this in the tool. Thanks for looking, Daniel Attachmentprojects(3).zip (782 Downloads) |
2/5/2010 9:00 AM | |
Posts: 4 Rating: (0) |
Thanks for the info Safety1, was wondering if the tool was really of any use with IEC61511 as you say. |
Follow us on