(0)| 2/26/2010 4:48 PM | |
|
Joined: 1/17/2007 Last visit: 11/20/2025 Posts: 1561 Rating:
|
The error code you are reporting would suggest that you are using Modbus TCP (with a 343-1 or 443-1). I believe that modscan32 is only for serial modbus (over RS232 / RS485). You require a modbus TCP simulator. The one you need will depend if the PLC is client (master) or server (slave). The two I have used in the past are:- The server simulator is a program called Mod_RSSim and is free. The client simulator is a program called Simply Modbus TCP Client and costs a small amount for the full version. There is a demo version that you can download for free. |
|
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
Follow us on