Industry Online Support
Technical Forum
8/20/2006 12:12 PM | |
Posts: 6 Rating: (0) |
Hi! I want to know how can I use the CP 341 in a distributed configuration (ET 200 M)? How can I parameterize the CP? |
8/20/2006 12:26 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi, The CP341 can be used in a decentral setup the same as in a local setup. However you have to look if the decentral speed is high enough. The blocks to do this are together with some examples to download in the next link: Download CD "CP340, CP341, CP440, CP441", version: V5.1+SP7 |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on