6/20/2010 6:24 PM | |
Joined: 9/18/2006 Last visit: 11/11/2024 Posts: 593 Rating: (64) |
Hi. If you had such problem it is necessary, this my opinion, I do not hurry :): 1) to try to establish connection Scout (Starter)-> CU320 2) to read errors and magazine of errors If necessary: 1) to start an automatic configuration 2) to load the equipment design in CU320. If at you it is not possible to establish connection Scout (Starter) with CU320 you can try to remove data of drives from a CF-card, and then again to try to establish connection with CU320. My opinion, if all LED red light, a problem in data on a CF-card (possibly) or hardware CU320 (is improbable). Probably it will help you. Best regards. AttachmentDescription of the LEDs on the Control Unit.pdf (514 Downloads) |
6/20/2010 6:39 PM | |
Joined: 9/18/2006 Last visit: 11/11/2024 Posts: 593 Rating: (64) |
Hi. This small addition. If the controller PLC-program probably has block OB82. In this block it is possible to change controller reaction. I hope it to you will help. Best regards. AttachmentDiagnostic Interrupt Organization BlockOB82.pdf (317 Downloads) |
Follow us on