8/30/2010 10:09 AM | |
Joined: 10/7/2005 Last visit: 10/3/2024 Posts: 3023 Rating: (1054)
|
Hellorelu18 Apart from the Stop in Event 11 (which was caused by "stop switch being activated")I think teh description for events 2,7 & 16 say it pretty clear:Power failure! I suggest you check thepower supply and/or its connections and hope this helps. |
Cheers |
|
8/30/2010 10:26 AM | |
Posts: 4 Rating: (0) |
Hello Fritz, I already changed the power suplay but with no rezult |
8/30/2010 10:48 AM | |
Joined: 10/7/2005 Last visit: 10/3/2024 Posts: 3023 Rating: (1054)
|
In that case I can only speculate that you have a faulty M7 CPU (or perhaps bad internal connections on its power supply terminals). Do you have a spare M7 (I hope, as they are hard to come by nowadays)? |
Cheers |
|
8/30/2010 10:50 AM | |
Posts: 4 Rating: (0) |
second problem is : When i make the Upload station to PG i have only the Hardware config . |
8/30/2010 3:09 PM | |
Joined: 9/27/2006 Last visit: 10/3/2024 Posts: 12283 Rating: (2685) |
Hello relu; Uploading blocks from a M7 requires a specific procedure. have a look at the M7 System Software manual, chapter 7: http://support.automation.siemens.com/WW/view/en/1136533 Hope this helps, Daniel Chartier |
8/31/2010 1:16 PM | |
Posts: 4 Rating: (0) |
Hello, I have only the Step 7 v5.4 in my PG, And for M7 RMOS32 I need windows 95? Thanks, |
Follow us on