9/26/2010 9:20 AM | |
Posts: 1 Rating:
|
Hello, I am seeking some help with the attached ladder diagram. I was given this diagram, and unable to ask further help from the author. Even though I understand the logic I dont have enough experience to program SoftComfort. The diagram includes initialising A, B and C =0 and then using these to sequence the logic. I am lost in trying to enter this into ladder logic or preferably FBD in Soft Comfort. Shift register or Flags may be a way to start.?? Any help would be most appreciated. regards Bagpress Attachmentbagpressladder.pdf (538 Downloads) |
Last edited by: bagpress at: 9/27/2010 9:15 AM |
|
11/19/2010 11:15 AM | |
Posts: 59 Rating:
|
Dear Bagpress I think your problem was solved now. But you check this program is suit for your application. This is one of way to write your program. I used counters and flags if you want another way you can program it that way. Logo module has some criticality of comparison so that you have to calibrate your Analog sensor as your set point requirements. Regards AttachmentLOGO!Soft Comfort - Circuit Diagram1.pdf (503 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on