12/6/2010 5:53 AM | |
Joined: 6/7/2010 Last visit: 7/9/2024 Posts: 571 Rating:
|
My controller is 6SN1121-0BA11-0AA1 with 200A LT module. |
Regards, |
|
12/6/2010 5:51 PM | |
Posts: 2964 Rating:
|
Hello.... What type of motor are you going to use....any i am attaching you the documents.. for ANA and Spindle... hope this will help you out... check it out.... Regards, Ekalavya AttachmentANA_611A sp.pdf (280 Downloads) |
This contribution was helpful to
1 thankful Users |
12/7/2010 6:13 AM | |
Joined: 6/7/2010 Last visit: 7/9/2024 Posts: 571 Rating:
|
Hello, 1PH7224-2NF00-0EA0 is the motor which i am using. |
Regards, |
|
1/7/2011 1:05 AM | |
Joined: 10/17/2007 Last visit: 7/14/2024 Posts: 4008 Rating:
|
Hi,friend,the info. for your motor:Siemens 1PH7224-2NF00-0EA0 Kompakt-Asynchronmotor, 100kW, 1500 1/min, 636.6Nm, 188 A,who make designing for the retrofitting ? howevery, if you cannot change the design. you need to have set up tool for SIMODRIVE 611U.try to do like that:1st of all saftey! make sure you spindle motor is ready to run in mechnically=lub.gear.OK, no clamping the tool;manully truning smoothly 2nd, you can control the 611 power module= using switches control 9-63/64/48/. and control on 611U:9-->663,9-->65, then hook the cable PC<--->611U, start SIMOCOM U in you PC,config.you spindle motor stet-by step, I think you know. and when you done. test run sp motor using SIMOCOM U. when it is running good. then try to use battery box(1.5VDC is OK) connecting to 56/14 to run your motor. when it is OK. at this point you can connect ANA to 611U, if the design is OK you should get: in 840D MDI mode, input:S500M03, then cycle start your spindle should run in 500rpm. about cable for encoder,i suggest you order Siemens cable DO NOT make or modify by youself. additional info. for you : if your design there is an encoder mech. connected to spindle gear sigal of this one should go to ANA, and encoder on spindle motor the sigal goes to 611U. if there is no encoder on gear box, then you config. 611u to spindle as no encoder. you connect motor encoder to ANA. REF# manual attached. good luck.
Hi, Yes you are correct , I am using 840D, PC50.3, We are retrofitting pama horizontal boring machine, machine is in final stage , its not possible to change the card for me.So i have to use the same card for the spindle.I have a dought wheather any run command is to give to drive for rotating the motor ? AttachmentFBAN_0200_en.pdf (250 Downloads) |
Last edited by: nulizhang at: 1/7/2011 1:25 AMLast edited by: nulizhang at: 1/7/2011 1:24 AMIf you like my comments please |
|
Follow us on