4/10/2011 6:50 PM | |
Joined: 6/7/2010 Last visit: 7/9/2024 Posts: 571 Rating:
|
Dear Eshwar, 1)Pin no: 36 is Forward/reverse command Parameter: P671= 11 P672=10 If we feed 24 V DC for pin no:36, Means reverse command. 2)Pin no: 37 is Run command 3)Pin no: 38 is Drive Enable (Emergency stop) 4)Alarm for Drive Fault: X171 pin no: 48 & 54 Parameter: P772 =106 As per you Requirement when press Start Push button ,in Pin no:37 &36 ,24VDC should be given. For Main contactor ,Find the attached drawing,As per that,drive automatically switch ON & Switch off the Contactor. Attachment6RA70.pdf (450 Downloads) |
Regards, |
|
4/14/2011 12:40 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello Eshwar,Please go thru the attached file. It will help you. AttachmentSimoreg 6RA70 start up procedure.pdf (499 Downloads) |
Follow us on