4/6/2011 1:14 PM | |
Posts: 197 Rating: (3) |
Thank u IBN-Service. I came across the following useful links: /tf/WW/en/Posts/32107 /tf/WW/en/Posts/50509 /tf/WW/en/Posts/42220 /tf/WW/en/Posts/38448 /tf/WW/en/Posts/50354 /tf/WW/en/Posts/36786 However, is there a way to do bit-by-bit increment at the rise of the pushbutton signal "I4.0" ......... something similar to my first post and without using LOOP command ? Thanks again. |
4/15/2011 12:33 AM | |
Posts: 32 Rating: (2) |
Hello You mean that i want to zero first three bits of accum so be byte pure so it is equal to p#byte.0 i hope iam alright regards |
Follow us on