8/12/2010 2:50 PM | |
Posts: 3 Rating: (0) |
Dear Ekalavya, Thank you for reply. I checked it out now and the connection is OK. Do you suggest me anything more? Best Regards AYBARS |
8/13/2010 10:41 AM | |
Posts: 2964 Rating: (482) |
Hello Aybars, I am not able to see the line filter in picture do youreally have it...your DIP swtich no 6 really matter beacuse the 6 is ON Sinusoidal current ( precondition you should line filter and choke) if 6 is OFF Square wave current. I am attaching the PDF of the same for the reference. I also checked all LT moduls+PW modul if there is any crack on PCB or loosining in copper bar screws.==> you will really have spark this should be corrected how is input supply connection given to the machine and I/R module? Does your Linefilter(6SN1111-0AA01-2CA0) and choke(6SN1111-0AA00-0CA0) are of same ratings of your I/R module Is this problem has started how? if it is failing like this there is really some problem in the wiring / mechnical load and control panel AC temperature check it out.... Regards, Ekalavya Attachment611A switch 1.6.pdf (423 Downloads) |
8/18/2010 8:55 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hi Aybars, Can you provide us the details (MLFB no) of power modules connected to ER module. DEEP |
Follow us on