Industry Online Support
Technical Forum
7/25/2011 11:29 PM | |
Posts: 59 Rating: (0) |
¿Se puede simular el panel de operador con un PLC s7-1200 Sin necesidad de simular con variables? |
7/26/2011 8:48 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166) |
Dear Johan, Have you seen this thread: /tf/WW/en/Posts/59537 and this thread: /tf/WW/en/Posts/34588 and this link: Why is communication between the Runtime simulation and the S7-1200 not possible if the PG/PC interface is not set correctly? Best regards, Wizard |
Last edited by: Wizard at: 7/26/2011 8:49 AM |
|
Follow us on