12/28/2006 12:07 PM | |
Posts: 13 Rating: (0) |
Hi guys, I have to config a Scalance (X208)and 315-2DP PLC comes along with a CP343 . If I do not config anything for the Scalance, just plug the Computer ethernet cable (RJ45) and PLC (RJ45) cable to the Scalance, there will be no error appear. But if I use the hardware config (in Step 7 Ver 5.3) to config the scalance, the errors appear. I did use the document (BA_Scalance-X100-200_76) and following these steps..but it doesnt work. Can anyone suggest any ideas how to config these ? I'm really new to this hardware (Scalance) Thank you alot PS: this link is the picture I capture after config and download to the hardware: http://farm1.static.flickr.com/130/336084712_5818748975_o.jpg |
Follow us on