8/20/2011 12:40 AM | |
Posts: 24 Rating: (1) |
Hello! Could someone please explain me how to initialize variables ? I need to make sure that each time that I run a function block or when I run the software for the very first time all the variables must be set to their initial values...I guess this is a basic question... but this is frustrating me! Thanks in advance!! ------------------------------------------------------- Edited: Im working with CPU 1214C. The closest I get to solve this problem is shown in the pictures below. When I try to set up the initial condition the field is not active... see attachment 1.jpg and 2.jpg I am also trying to initialize local variables doing this way: see attachment 3.jpg But it is not working... i find some strange behaviors in the local variables... for sure Im doing wrong here!!!!! Attachmentpictures.zip (585 Downloads) |
Last edited by: O_Moderator at: 8/21/2011 10:43 AMpictures transferred to attachment Last edited by: RichardSapp at: 8/20/2011 9:16 PM |
|
8/23/2011 6:47 PM | |
Posts: 24 Rating: (1) |
Many thanks! |
Follow us on