9/3/2011 7:32 AM | |
Joined: 8/9/2011 Last visit: 11/1/2023 Posts: 324 Rating:
|
Yeah I got it![]() I was thinking of doing the same otherwise.
In SWITCH instruction can u give your own name or its mandatory to name it like LABEL0, LABEL1 and so on? If its mandatory what if we use two SWITCH instructions in the same block as far as naming of the labels is concerned? After compling it gives an error message "The element is not supported in this language version" The same message you will get if you use JUMP_LIST too.?Ours is step7 basic professional(Trial version) Network 7: LABEL Instruction body …. …. …. JUMP to LABEL It will jump to LABEL if the condition is met. My doubt is whether the instructions after LABEL get executed at first scan or they are bypassed waiting for the JUMP to execute first? I mean to say is it the case that the label instructions are executed only if JUMP does? Please refer the file. Thanks AttachmentFB.zip (588 Downloads) |
"Any intelligent fool can make things bigger, more complex. It takes a touch of genius -- and a lot of courage -- to move in the opposite direction.":):) |
|
This contribution was helpful to
1 thankful Users |
Follow us on