9/9/2011 4:51 PM | |
Posts: 22 Rating:
|
Hi! I have SINAMICS CU230P-2DP, V4.4 and IOP,data: firmware 01.01.17.00 ; bootloader 01.01.13.00 ; menu description 01.00.00.10; parameter description: 04.30.28.00 With CU230P-2DP V4.3 i can see all read-back parameters but when I connect CU230P-2DP V4.4 and IOP, there is on IOP start screenwhere should be decimal numbers and parameter name - "?????", "empty" In this page https://support.automation.siemens.com/WW/llisapi.dll?query=51445357&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx&lang=en&siteid=cseus&objaction=cssearch&searchinprim=&nodeid4=20229805 is given IOP V1.1 HF2 so that IOP could support the SINAMICS Firmware V4.4. I have doneupdate (HF2)successfullythrough PC but when im connecting back IOP and Control Unit V4.4, there is still"?????", "empty" IOP data is still same asdescribed above (parameter desc.) Has anyone any idea of it? Regards, Bezout |
9/12/2011 12:47 PM | |
Posts: 22 Rating:
|
Hi! I wrote to Support Request andseems thattheyimprovedtheir IOP V1_01 HF2. And its working, so ifanyone had/have same problem: http://support.automation.siemens.com/WW/llisapi.dll func=cslib.csinfo&lang=en&objid=51445357&caller=view Entry ID:51445357 |
Last edited by: bezout at: 9/12/2011 12:48 PM |
|
Follow us on