Industry Online Support
Technical Forum
10/28/2011 10:19 AM | |
Posts: 206 Rating:
|
Hello Ni Lar, the task you want to do is a little more complicated tha a standard calibration. I suppose that the scale indicates the weight of the liquid inside. 1. You have to read the actual digits (see shot "digits.jpg) and note them. 2. Remove the pump. 3. Read the new actual digits and note them. 4. Calculate the difference between the digits and note it. 5. Read all data from Siwarex U (see shot "read_all.jpg) 6. Go to DR3 (DR4 for channel 2) tab "Adjustment digits" 7. Subtract the differnce from 4. from "Adj. digits 0" and "Adjustement digits 1" (see Adj.jpg) 8. Send DR3 (DR4 for channel 2). Now the Siwarex U should show the actual weight like before. Regards ABenno Attachmentshots.zip (111 Downloads) |
Follow us on