11/4/2011 1:05 PM | |
Joined: 4/22/2010 Last visit: 10/17/2024 Posts: 5697 Rating: (715) |
Hello In Step7 v5 there are some rules to present the program inLAD or FBD, that is just for showing the networks on the screen, the PLC don't care about that if it compiles and download it's o.k. for the PLC. Here a link to explain a bit about it: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=21952992&caller=view Scroll a bit down. So if the compiler accepts your code it's o.k. to do it. Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
11/4/2011 2:32 PM | |
Posts: 5225 Rating: (1195) |
This method goes against my "old school" training. It is all good if the compiler accepts it. Thanks to both of you who responded. --William |
Follow us on