8/3/2010 1:15 PM | |
Posts: 17 Rating: (3) |
Dear Tomy The S7-1200 will support a embedded Web Server with mail forwarding functionality this new feature will be available at Nov or Dec with just a firmware update :), this update is cost free. until then we have to use the CE-25 the SMS send and received feature http://support.automation.siemens.com/WW/view/en/40616248 Best regards, |
Last edited by: tokzu23 at: 11/7/2011 4:30 PMalmost 1 year latter... This innovation for the S7-1200 is been discharge the S7-1200 wont have Mail forwarding directly it could be posible using external mailserver via ethernet standard |
|
This contribution was helpful to1 thankful Users |
10/17/2011 5:09 PM | |
Posts: 126 Rating: (18) |
Service Pack 2 should contain a block for sending e-mails either through ethernet or through the Teleservice Adapter IE Basic. |
12/7/2011 8:25 AM | |
Posts: 4 Rating: (0) |
Is the web server email capability ready it is december? i have an large opportunity at a OEM if it is |
12/7/2011 8:27 AM | |
Posts: 4 Rating: (0) |
Do you haveexample codesending emails |
12/22/2011 11:27 PM | |
Posts: 39 Rating: (1) |
Hi TIA 11 SP 2 has the TM_MAIL function «Send an e-mail to an e-mail server» seein STEP 7 Professional V11.0 SP2 or STEP 7 Basic V11.0 SP2 published ~12.12.2011. enjoy salu_ |
This contribution was helpful to1 thankful Users |
Follow us on