12/19/2011 7:17 AM | |
Joined: 10/3/2010 Last visit: 7/31/2024 Posts: 1560 Rating:
|
As it says in the description of the FAQ, it's a change that you can add to the registry if you get the message "Could not start/terminate Alarm Logging in allotted time" or "Could not start/terminate Tag Logging in allotted time" when you activate/deactivate WinCC. If it just takes times to terminate Run Time, I don't think changing this timeout for Runtime will help you at all. If you really want to try, it says that you have to add a DWORD called "Application Deactivation" for creating a new timeout value for terminating Runtime and a DWORD called "Application Activation" for a timeout when starting RT. As you can see in your attachment, those parameters are not in your registry by default. |
B r g d s , |
|
12/19/2011 2:42 PM | |
Posts: 1776 Rating:
|
Hi, have you done the changes as SteBo and Tagolover and the FAQ mention? Do you get a better result? http://support.automation.siemens.com/WW/view/en/268850 |
12/20/2011 8:05 AM | |
Joined: 10/3/2010 Last visit: 7/31/2024 Posts: 1560 Rating:
|
That's how Windows Registry works, don't worry. You can see your decimal input between brackets at the end. |
B r g d s , |
|
12/22/2011 11:40 PM | |
Joined: 11/12/2008 Last visit: 7/8/2024 Posts: 180 Rating:
|
THANKS ALOT |
HASSAN.S POJAILA |
|
Follow us on