1/16/2012 10:06 AM | |
Posts: 39 Rating: (0) |
Dear all experts Im facing some problem while doing programming with S7-1200 programming software "TIA". 1. Im not able to do absolute addressing with local data of FB block interface.While doing so S/W is showing error, i.e "ABSOLUTE ACCESS TO LOCAL DATA STACK NOT PERMITTED". 2. Also address of local data is not given in local memory of FB/FC, as it is given in S7-300 S/W. Im attaching the S/W program and pdf file, which will elaborate my querry. Thanks&Regards Zakir Sayed
AttachmentERROR1.pdf (538 Downloads) |
1/19/2012 8:16 AM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating: (136) |
Hello, I'm not sure, but it could be possible that this feature is solved with the installation of SP2 (STEP 7 TIA Portal V11+SP2). Otherwise ask the customer support (hotline) from Siemens. See the link for make an service request: http://support.automation.siemens.com/WW/view/de/38716036 With best regards |
1/19/2012 4:54 PM | |
Joined: 4/24/2006 Last visit: 10/3/2024 Posts: 8744 Rating: (1168) |
Hello, Here you can download SP2: Service Pack 2 for Step 7 V11 Service Pack 2 for WinCC V11 Best regards, Wizard |
1/19/2012 5:24 PM | |
Posts: 39 Rating: (0) |
Dear Wizard Thanks, but im looking forSTEP 7 TIA Portal V11+SP2.Pls could you do the needful. Thanks & Regards Zakir Sayed |
Follow us on