Industry Online Support
Technical Forum
1/23/2012 7:51 AM | |
Posts: 17 Rating:
|
I did a project using the S7-1200 and MD741 and S7-1200 from within the web-server enable. and used a block of www . Without md741, when connected directly to the S7-1200 is running the web page. But does not work when connected via MD741. I did all the port forwarding in MD741, but not working. S7-1200 can be delivered online over MD741 and I know programming. S7-1200 IP address of 192.168.2.3. MD741 in the external IP address of 188.234.23.45 AttachmentMD741_setting.pdf (226 Downloads) |
1/23/2012 10:21 AM | |
Posts: 1547 Rating:
|
Hi, maybe you connect via HTTPS? So you have to forward port 443, too. |
1/23/2012 1:27 PM | |
Posts: 17 Rating:
|
Hi; I connect to the remote S7-1200. but I can not open web page in the S7-1200. |
Follow us on