Industry Online Support
Technical Forum
2/21/2007 3:34 PM | |
Joined: 9/23/2005 Last visit: 10/2/2024 Posts: 4348 Rating: (1446) |
[quote user="Biram"]Dear Experts Need your help. We have one PCS7 redundant system where the CPU shall be placed in two different control room and 2 different Panel. The CPU type number is 6ES7 417 4HL04 0AB0 . I want to know following things. What will be the MLFB number of Sync module in this case. What will be type number of Sync cable for 500 meter distance. Also let me know, is there any single MLFB number in PCS7 family which have above two MLFB's. Regards Bikram bikram.bhattacharjee@foxindia.net Hi, Sorry, I don't find the PCS7 order nunber, but I find the information in the Catalog ST70 (www.siemens.com/simatic/printmateria), page 5/44: Sinc module 6ES7 960-1AB04-0XA0 / cable, just on request. |
Denilson Pegaia |
|
3/11/2007 2:13 PM | |||
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Dear Bikram, You need the long distance modules, these have the MLFB-number:
The cable you want, you have to order by a external supplier, Daetwyler for example: http://www.daetwyler.net/d/index.htm I don't know if this can be ordered at once, I think the AS could be ordered but the FO-cable would be ordered by a external supplier. Please ask on the PCS7 forum if there is one number for the AS with the -1AB04 Sync Modul. |
||
Last edited by: Late at: 11.03.2007 14:16I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|||
Follow us on