5/5/2012 12:08 PM | |
Posts: 327 Rating: (28) |
Greetings Can you rephrase you question, it is not very sensible? Best regards
|
5/8/2012 12:17 PM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242)
|
As I understand, when you try to open Step-7 v5.4, V11 wants to be closed ? Maybe you have some error message ? Indeed it is compatible on one computer as its stated here . When you tell us that V11 wants to restart or close I think it generates and error. This should be send to a support together with a diagnostic folder. Open support case as it is internal error of V11. By the way, did you installed SP2 for V11 ? Service Pack 2 for STEP 7 V11 Updates for STEP 7 V11 SP2 and WinCC V11 SP2 |
Best regards, |
|
5/8/2012 12:36 PM | |
Joined: 7/13/2010 Last visit: 8/21/2024 Posts: 7 Rating: (0) |
My OS XP sp3 |
Follow us on