5/24/2012 8:49 AM | |
Posts: 131 Rating: (4) |
i need to learn scl language is ther manual here for SCL language? |
5/24/2012 9:04 AM | |
Joined: 8/31/2010 Last visit: 9/30/2024 Posts: 1522 Rating: (228) |
Hello boazeventall, Right now there is no getting started type of manual for SCL in TIA Portal. Still there is a S7-SCL V5.3 for S7-300/400 Getting Started (quite old one). You have to adapt it for TIA Portal. |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
5/24/2012 9:56 AM | |
Posts: 1064 Rating: (72) |
You can call the fc fb from ob1 either conditional or unconditionaly |
5/24/2012 11:13 AM | |
Joined: 3/24/2009 Last visit: 7/9/2024 Posts: 535 Rating: (112) |
Dear boazeventall, on a 300/400 cpu you can access the db-tag with db2.dbw0, but on a 1200-cpu with optimized block-code you have to use the symbolic access. To use the absolut-adress-access the code-block and the data-block have to be created with 'standard - cpu300/400- compatible'-attribute. Best regards, yy1 |
Last edited by: yy1 at: 5/25/2012 12:29 PManswer is related to question in /tf/WW/en/Posts/75167 |
|
Follow us on