5/23/2012 10:42 AM | |
Posts: 18 Rating: (0) |
Thank you so much for your understanding and helping, I solved that problem.The Motors(1,2,3) run respectively. What I mean that is M1 runs for 5s.After M1 is off,M2 runs for 5s.After M2 is off,M3 runs for 5s..And this system will be go on Until I press the stop button.... So I solved What I say above problem..Actually my aim is to add some contact just like I0.1,I0.2,I0.3.The summary of the purpose of the program is following Firstly,The motors will be run as above,respectively but, 1)when I press the I0.1,the m1 will be off and the other motors that motor2 and motor3 will be run respectively(5s M2, 5s M3 and continue like this until when I press the stop button)..And The system will be run as before If I give up pressing to I0.1 button 2) When I press the I0.2 the M2 will be off....and same process 3)When I press the I0.3 the M3 will be off....and same process The file contains the M1,M2,M3 running respectively but dont contains I0.1,I0.2,I0.3 buttons please help me,thanks Attachment3MotorsRUN_respectively.zip (396 Downloads) |
5/23/2012 4:51 PM | |
Posts: 18 Rating: (0) |
yes I need how can I put the input contact to satisfy the condition. I0.1 for M1 I0.2 for M2 I0.3 for M3 you could make? pls help |
5/23/2012 6:43 PM | |
Joined: 2/16/2011 Last visit: 7/8/2024 Posts: 229 Rating: (28) |
Hello, I did some modifications in the sample in attach.. I hope it helps Regards
Attachment3MotorsRUN_respectively_2.zip (445 Downloads) |
Gabriel de Oliveira |
|
This contribution was helpful to1 thankful Users |
5/24/2012 12:04 PM | |
Posts: 18 Rating: (0) |
The new and last version.Thank you so much Gabriel, My purpose is ok.
AttachmentLAST_OF_LAST_3MOTORS_APPLICATION.zip (447 Downloads) |
Follow us on