Industry Online Support
Technical Forum
5/24/2012 11:13 AM | |
Joined: 3/24/2009 Last visit: 7/9/2024 Posts: 535 Rating: (112) |
Dear boazeventall, on a 300/400 cpu you can access the db-tag with db2.dbw0, but on a 1200-cpu with optimized block-code you have to use the symbolic access. To use the absolut-adress-access the code-block and the data-block have to be created with 'standard - cpu300/400- compatible'-attribute. Best regards, yy1 |
This contribution was helpful to2 thankful Users |
5/25/2012 12:08 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already discussed in the following thread learning scl language Best regards O_Moderator |
Follow us on