Industry Online Support
Technical Forum
10/11/2005 11:05 AM | |
Joined: 8/25/2005 Last visit: 7/5/2024 Posts: 1161 Rating:
|
Hello Nestor, I copy the information from HW-Config for you: "6GK7 343-1GX11-0XE0 S7 CP for Industrial Ethernet ISO and TCP/IP with SEND/RECEIVE and FETCH/WRITE interface, long data, UDP, TCP, ISO, S7 communication, routing, module replacement without PG, with web server and E-mail, 10/100 Mbps, fixed MAC address, initialization over LAN, IP multicast, NTP, FTP, firmware V2.0" so I'm sorry, but the CP you are using don't have PROFINET functionality. I think you need the CP343-1(order no. 6GK7343-1EX21-0XE0) Here a Link to the Product Support were you will find more information's about this CP: New CP 343-1 Communication Processor Released for Delivery (PROFINET-Controller) Best regards Sabine |
Follow us on