5/15/2007 2:39 PM | |
Posts: 25 Rating: (3) |
Dear all, I have used SFC 51 to display the h STATUS using the SZL ID 0071 and configured in the HMI for Displaying the Status. Could any one please tell me how to display the IM 153-2 Active LED Status in the HMI? Can any OB 83 can help?? AttachmentIM 153-2 Active LED Display.zip (742 Downloads) |
5/15/2007 10:22 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi, Please read out the diagnostic status with SFC13 and look in the handbook Distributed I/O Device ET 200Mand see 9.3.9 H status (only with S7-400 H and normal redundancy) withfigure 9-6 on page 9-20. The boolean "IM 153-2 in data exchange" on "1"is the IM 153-2 with the active LED. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on