(1)| 10/26/2012 10:45 AM | |
|
Posts: 664 Rating:
|
Hai MBA, Thanks for the great reply, Please can u tell me What is PIservice =P#DB16.DBX 360.0 BYTE 14?? Thanks&Regards, Raj
|
| 10/29/2012 4:26 PM | |
|
Posts: 391 Rating:
|
A pointer for "PI".LOGOUT PIservice ="PI".LOGOUT |
| 1/29/2013 7:08 PM | |
|
Posts: 159 Rating:
|
I am a novice atthisbut thought I would try this as a project.However Iam having some issues. Can anyone help? Please explain in"beginners" fashion!! I created a new FB212. In the first network I havean input from the MCP I4.0 to makea local output marker #PWORDCOIL go high. In the second network I am trying to use this marker to insert the SUNRISE password via a local variable input STRING[8] called #PW. Like so - CALL "PI_SERV", DB200 Req:="PW_DB".PWORDCOIL PIService:="PI".LOGIN Unit:=1 Addr1:=DB300.DBX0.0 DB300 is the instance DB of this FB212. This sits okay with no errors when downloaded to the machine tool. When I try to call this FB from OB1 I am getting the red error messages in the relevant attachment. I think the variables match what is requested but I can not get it to work. I have also attached my local variable workings. HELP? Thanks in advance, Craig. Attachmentpassword_fail.zip (433 Downloads) |
Follow us on