4/25/2007 5:21 AM | |
Posts: 38 Rating:
|
Hi stleric, If i´m not wrong, the only thing you have to do to make a recursive possible is to add a flag after the block you need to send back in the program, and do the recursive from this flag output I´m not completely sure if this was what you ask for Best regards KLooPY See the attach, there is a sample program Pay attention on the fact that I think that you can not set 8 block in the same line (I do not remember if that restriction is still in use or if was used in older versions) AttachmentOI_2005_LCP.zip (1256 Downloads) |
Follow us on