Industry Online Support
Technical Forum
8/13/2013 1:27 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello, In addition to Amit_86's answer: Yes, when you have a file with extension .psr it is a backup file from an old panel, see the following link: how to Backup and restore a program on a text or graphic-based panel? This can not be restored on an OP77B When you want to migrate the project, you need the original project. Or start all from the beginning. Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
Follow us on