Industry Online Support
Technical Forum
8/14/2013 2:36 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi MRishikesh, The channel is enabled for the transfer, MPI / PROFIBUS ON TP 270? |
8/14/2013 2:47 PM | |
Posts: 166 Rating: (1) |
Yes sir it is enabled with a tick mark |
8/14/2013 3:26 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi The address is right? How do you read the current MPI / PROFIBUS address on a Windows CE panel? |
8/16/2013 6:56 AM | |
Posts: 166 Rating: (1) |
Sir As shown in the link sent by u , address under MPI is 1, we are selecting MPI only to connect and transfer Regards, M. Rishikesh |
8/16/2013 7:12 AM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hi What does that mean? does it work? |
Follow us on