Industry Online Support
Technical Forum
10/20/2013 11:31 PM | |
Joined: 9/27/2006 Last visit: 7/24/2024 Posts: 12270 Rating: (2676) |
Hello Parthiban.R; This Siemens brochure suggests the Sinamics G150 for an extruder: SINAMICS drives - Siemens SINAMICS® G150 is the Siemens drive solution for applications that do not require regenerative feedback into the line supply. These are predominantly applications with square-law load torque characteristics – i.e. pumps, fans and compressors, but also constant-torque applications such as extruders, mixers and crushers. voltage rangesSINAMICS G150 Power and voltage rangesSINAMICS G150 380–480 V 110–900 kW 500–600 V 110–1,000 kW 660–690 V 75–1,500 kW Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/20/2013 11:32 PM |
|
Follow us on