Industry Online Support
Technical Forum
9/20/2012 9:30 AM | |
Joined: 4/24/2006 Last visit: 10/3/2024 Posts: 8744 Rating: (1168) |
Hello v_nemec, Here are some links, perhaps they are useful: In STEP 7 (TIA Portal) V11, how can you input, read out and edit the date and time for S7-300/400/1200? Which functions are available in STEP 7 V5.5 and in TIA Portal V11 for processing the data types DT and DTL? how do you synchronize the date and time between an operator panel and an S7-300/S7-400 controller with WinCC flexible? Best regards, Wizard |
9/26/2012 10:50 PM | |
Posts: 3 Rating: (0) |
Hello Wizard, thanks for the links, but I already saw them, I tried uploading new firmware into S7-300 (version 3.2.7), but it's still the same, Siemens support said the program is ok. I'm getting mad and have lost so much time with that damned clocks. Any other ideas than destroying the panel? I'm attaching the project in case someone will be so nice to check it. AttachmentProject2.zip (322 Downloads) |
10/24/2013 4:19 PM | |
Posts: 1299 Rating: (136)
|
Hello adamgresch, did you check the links Wizard posted above? K!ke |
Follow us on