1/24/2014 5:52 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating:
|
Hello, Let's start with the difference between FB and FC: The S in front off FB or FC stands for System, these are blocks build in the PLC, no need to download them (you can't, download button is greyed out). All blocks are used to organise the program or to not have to program something yourself but use a standard block. In your library you will find also standard FC and FB i.e. PID or Scaling, Regards, Marcjan |
Problem solved? |
|
1/30/2014 2:54 PM | |
Joined: 9/1/2005 Last visit: 8/12/2024 Posts: 4104 Rating:
|
follow up question published bysultanahmedis split to a seperate thread with the subject sample project of FC ,FB and SFC/SFB Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on