Industry Online Support
Technical Forum
2/7/2014 12:01 PM | |
Posts: 16 Rating: (0) |
Thank you I am using WinCC flexible 2008 SP3, I will connect 2 PLC's with an ethernet switch. |
2/8/2014 9:15 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
... 6 axis aren`t a problem with a S7-1200. You can use SINAMICS G120 drive with a CU250S. So you can use the basic positioner inside the CU250S and send the setpoints over PROFINET. In the following link you will find the "FB284": http://support.automation.siemens.com/WW/view/de/68034568 If you want to use a SINAMICS S drive (with CU305 for example), they would be the same FB284. |
Follow us on