8/26/2011 9:22 AM | |
Joined: 1/28/2009 Last visit: 8/26/2024 Posts: 6846 Rating:
|
Dear member For more information on classical 3-term PID controllers refer to the following links: Also check following thread for sample program for FB41 and SFB41.I think the samples would be a good starting point to get the basic information.Also you can get the official description of the function, select the function in SIMATIC Manager and press <F1>. FB41 PID exampleBest regards Attachmenthd_FB41_EX.zip (2681 Downloads) |
Last edited by: hdhosseini at: 12/10/2018 9:03:28 PM |
|
This contribution was helpful to
1 thankful Users |
8/28/2011 9:06 AM | |
Joined: 8/18/2011 Last visit: 9/9/2022 Posts: 14 Rating:
|
Dear sir. hdhosseini, Hope your doing fine now, thank you for giving me the right example for using PID..its giving me the right way how to use the PID... God Bless You always... Best Regards, HRAY. |
This contribution was helpful to
2 thankful Users |
1/7/2013 5:35 PM | |
Posts: 1 Rating:
|
How can I use this function block to control speed of DC motor?How can I do this?Is there anyone do this before? |
3/24/2014 7:42 AM | |
Posts: 340 Rating:
|
new question is splittet to How to use FB41 with one analog input and one analog output signals? |
Follow us on