8/26/2014 2:59 PM | |
Posts: 215 Rating: (6) |
Hi Fredmans, one LOGO! can act both client and server. install for for each communication between two LOGO!s 0BA7two connections. Follow the menu Tools>Ethernet connections Click right on Ethernet Connections and add connection The parametrerisation has to be - one connection as a master - one connection as a slave Do also for the communication partner. For details look up the example Residential Home Application with Weather Station on site Application examples for LOGO! Regards |
Follow us on