9/5/2014 8:36 PM | |
Joined: 7/15/2009 Last visit: 7/31/2024 Posts: 30 Rating: (0) |
and this is the original faceplate with all properties ... |
9/9/2014 8:31 AM | |
Posts: 1299 Rating: (136)
|
Hello abosama, There are different devices on which your wincc system can run in the end: Panels, PC with Runtime Advanced and PC with Runtime Professional. Depending on this device you need a specific version of WinCC (TIA Portal). If your device will be a Runtime Advanced or a Panel you have the right version of TIA Portal. If your device will be a Runtime Professional system you'll need WinCC Professional. http://support.automation.siemens.com/WW/view/en/99684510 If you just want to create faceplates for a Runtime Advanced system or a panel you have the right version and you can create faceplates. Just click "OK" in the dialogue of the first picture. K!ke |
9/11/2014 9:53 AM | |
Posts: 1299 Rating: (136)
|
Hello, What do you mean with "but when i operate the advanced Runtime screen then click on my pump i have nothing "? here is a very good description: http://support.automation.siemens.com/WW/view/en/68014632 K!ke |
Follow us on