Industry Online Support
Technical Forum
10/28/2014 9:06 AM | |
Joined: 5/12/2006 Last visit: 7/30/2024 Posts: 22330 Rating:
|
Hello, for SINAMICS you can use the STARTER SW, is free of use. At the moment o looks that the communication between the PLC and the drive is not working. Can be that any cable is damaged, or the PLC project is not loaded etc. In such a case you should contact your supplier for help. Regards Christoph |
10/30/2014 8:06 AM | |
Joined: 5/12/2006 Last visit: 7/30/2024 Posts: 22330 Rating:
|
Hello, with a card reader you can check if the Filesystem is ok or not (is simple FAT formated). Regards Christoph |
Follow us on