2/17/2015 2:32 AM | |
Joined: 2/20/2014 Last visit: 6/11/2024 Posts: 396 Rating:
|
HI, i am trying to a aeration pump control message display (run timer setting, remaining timer) and also total run time for each pump. I am having problem with the program that i have with me currently. The problems is that the pump 1 (Q1) starts to run once when the program is transferred to LOGO before the I1 is activated. I will attach my program here. Please do help me on how i can fix this. Thank you. AttachmentLOGO!Soft Comfort - PWST_3_1_WS_TRT_2.lld.pdf (237 Downloads) |
2/23/2015 2:44 AM | |
Joined: 2/20/2014 Last visit: 6/11/2024 Posts: 396 Rating:
|
Need your help, Sorry for the late upload of the program as i didn't know that i have zip and upload the program file. I actually wanted to get total run time at the webserver TD, i am able to achieve that but now the only problem is that the output Q1 is energized even without me triggering the input I1. In simulation it works fine but when i transfer the same program to the LOGO and test it with LED, the LED is turned on before I1 is true. I have tried changing the pulse generator block where the LED is steady all the way even without turning on the I1. So please help me. Thank you in advance. AttachmentPWST_3_1_WS_TRT_2_n.rar (216 Downloads) |
2/24/2015 3:24 AM | |
Joined: 2/20/2014 Last visit: 6/11/2024 Posts: 396 Rating:
|
Hi, i managed to fix the issue, it was because of the message text function block. and the coil which i had used to connect the output of the message text block. Now i have another problem which i am looking for a fix. In the same program which i had uploaded earlier, i had used the counter function block to count the time value in seconds, minutes & hours separately. I just noticed that the minutes value is not increasing after 1 minutes, meaning when the seconds value reach 60, the minute value becomes 1, but when the seconds value become 120, the minutes value is not increasing to 2 and so on. Please help me to fix that. I will upload again the update file.AttachmentPWST_3_1_WS_TRT_2_TTF.rar (200 Downloads) |
Last edited by: karthikk at: 2/24/2015 3:24:52 AM |
|
Follow us on