1/24/2006 9:30 AM | |
Joined: 8/31/2005 Last visit: 10/22/2024 Posts: 2198 Rating: (328)
|
I think the article with ID 6741018will help you. |
|
|
1/24/2006 1:16 PM | |
Joined: 8/31/2005 Last visit: 10/24/2024 Posts: 217 Rating: (41) |
Hi Dimbas! I don't know, if I understand you right... You have a "real" CPU414-4H, firmware version 3.1.1 and in your HW Config you can only find the CPU414-4H with the firmware version 2.1? With STEP 7 V5.2 or higher you have the possibility to update the hardware catalog of the HW Config via the internet. Just open HW Config and execute the hardware update via: "Options -> Install HW Updates ...". If you have an older version of STEP 7 updates of the hardware catalog can only be done with the installation of service packs. But it is always recommended to have the newest service pack installed. Check this link for the STEP 7 service packs: http://support.automation.siemens.com/WW/view/en/10805384/133100). |
Last edited by: Chris at: 1/24/2006 1:22 PMLast edited by: Chris at: 1/24/2006 1:22 PMGreetings, Chris |
|
Follow us on