(1)| 5/14/2016 3:40 PM | |
|
Posts: 4620 Rating:
|
Dear byrono, sorry if I intruding, I have never opened a CPU1200 but the specifications of the CPU 1215C says if you look belowon the tab Timers, Counters and code blocks supported by the CPU 1215C in Table 3 "Power supply" says: Internal fuse, not user replaceable 3A 250V, slow blow, then I wonder: are you sure it is the right CPU and not something else? SIMATIC S7 S7-1200 Programmable controller I think it's more a resettable fuse |
| 5/16/2016 4:03 PM | |
|
Posts: 5225 Rating:
|
Hi Byrono, Sorry to hear about the trouble you are having. Many factors can lead to failures - I assume you have a good 24Vdc power supply and is guarded against excessive EMF influences.
Seeing that this is a forum for Siemens industrial equipment users, I doubt you will get the clear answer you hope for. To speak directly to Siemens at - SIEMENS SUPPORT. In our age of mass production, this kind of occurrence is unfortunately not unheard of. The internal tracks of the PC board may have a crack somewhere that contributed to the failure - for example. I have had such problems before with Siemens.. but to be fair I have had such issue with Japanese and USA brands too. Normally there is a 6 month or so warranty on equipment such as this.. find out if you can claim. Maybe you can ask them to investigate the cause (autopsy) and make a report to you with recommendations. |
This contribution was helpful to
|
|
Follow us on