7/18/2016 4:04 PM | |
Posts: 10 Rating: (0) |
hello, can you help me out with static and dynamic connection. i am trying to connect 13 LOGOs, one as master others as slave. are these setting be made in logo soft. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/19/2016 1:49:13 AMNew subject after splitting |
|
7/19/2016 7:36 AM | |
Joined: 12/18/2014 Last visit: 11/8/2024 Posts: 34177 Rating: (4256)
|
Here is the project file for the screenshot.
Attachment13_0BA8_with_static_connections.zip (305 Downloads) |
This contribution was helpful to2 thankful Users |
7/19/2016 8:34 AM | |
Joined: 12/18/2014 Last visit: 11/8/2024 Posts: 34177 Rating: (4256)
|
Are the DIs push buttons or Switches? |
7/19/2016 8:54 AM | |
Posts: 10 Rating: (0) |
Push buttons |
7/19/2016 10:35 AM | |
Joined: 12/18/2014 Last visit: 11/8/2024 Posts: 34177 Rating: (4256)
|
Here is the complete solution.
Attachment2_master_with_11_slaves.zip (357 Downloads) |
This contribution was helpful to1 thankful Users |
7/19/2016 12:20 PM | |
Posts: 10 Rating: (0) |
Thank you, i really appreciate your help |
This contribution was helpful to1 thankful Users |
Follow us on