4/18/2008 6:46 AM | |
Joined: 3/26/2008 Last visit: 9/6/2024 Posts: 51 Rating: (0) |
should be the following axis enabled in follow-up mode or as leading axis follow-up disabled? |
4/18/2008 8:53 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3007)
|
Hello, the following axis cant be enabled as leading or following. All Axes are enabled normal, the synchronous operation is implemented over the following object an the command _enableGearing. I have attached a little program for test. Regards Christoph Attachmenttest.zip (689 Downloads) |
Follow us on