8/22/2016 1:05 PM | |
Posts: 35 Rating: (3) |
I have created in DB three status bits for indication my Pump status OFF ON Trip attached is my DB. is there another good idea you can provide me Best Regards, |
8/23/2016 6:30 AM | |
Posts: 144 Rating: (7) |
Hello Ali You can use Status Display object from the object pallet to monitor multiple statuses.Just need to create your desired states and then configure the Status Display object . More help here: Status display You'd better refer to WinCC manual and for that special subject( Dynamization ) the link below may be helpful: |
Last edited by: r.ethernet at: 8/23/2016 6:31:07 AM |
|
This contribution was helpful to1 thankful Users |
9/6/2016 7:14 AM | |
Posts: 144 Rating: (7) |
Hi ALi These two links below might be what works for you: Defining the color of objects with VBS More examples of VBS: |
Follow us on